I am getting some odd behavior while programming registers as well as a large amount of jitter on my locked output. I am tuning the evaluation board to my desired frequency, then copying the memory map to my own PCB.
When programming the registers, there are 4 registers that if I do not write the default values listed in the datasheet, the device does not work. As long as these registers have their default values written, everything works fine other than the locked output having a large amount of jitter that is not seen on the evaluation board. I have copied the evaluation board circuit on my PCB and have the 91 ohm resistor as suggested in the datasheet.
Here are the registers and their listed default values that I am having to write to get my 12.5 GHz output locked to a 10 MHz reference input:
Edit Notes
typo[edited by: HWalker553 at 8:28 PM (GMT 0) on 9 May 2019]