adjust the relative output phase of the ADF4355-2 for integer N.

Hi all,

Is possible to adjust the relative output phase of the  ADF4355-2 on each Register 0 update when N is integer, i.e. when the VCO output is integer multiple of the reference input?  Does ADF4355-2 support this feature all?  The following setting seems to work fine with FRAC N, but it has not effect for Int. N.

1. Autocal:  disabled.

2. RD:  disabled.

3. Phase resync.: . disabled.

4.  Phase adjust:  enabled

Thanks for the help,

Gmicael