ADL5205 Maximum input voltage swing

Hello,

I'm using the ADL5205 for a new design.

I have a doubt regarding the Maximum Input Swing of the ADL5205. While in page 3 of the datasheet specifies that the Maximum Input Swing is 8Vpp, in the absolute maximum ratings of page 6, the datasheet states that the Differential Input Voltage ((VINx+) − (VINx−)) is +-1V. Both informations seem contradictory. ¿What is the true maximum input swing?

My concern is about the maximum input level that the device can tolerate without damage (it doesn't matter if it is in linear operation or saturated) for the whole range of gain codes.



Thank you.

Joan Ramon

Parents Reply Children