Post Go back to editing

Mixer and LNA output connection IC-LT5500

What is the purpose of the LC circuitry connected at LNA_OUT pin and MIX_IN pin in the evaluation board in the datasheet? I want to connect the LNA_OUT to the MIX_IN. As described in the datasheet I need to connect an interstage filter between the two pins or I can use RC combination. CAn you provide me with more information about this filter or RC combination?

can you please provide me the number of resistance, capacitance an inductor value.

Is transformer necessary for output port or not?

Parents
  • FormerMember
    0 FormerMember
on Apr 15, 2019 1:11 PM

The LC networks provide 50-ohm matching to the mixer and LNA ports in addition to some filtering. Some inter-stage filtering should be included in your circuit. You have to design your own filter based on your system requirement.

The transformer is for differential to single-ended conversion. You do not need it if you are are taking the output differentially.

Reply
  • FormerMember
    0 FormerMember
on Apr 15, 2019 1:11 PM

The LC networks provide 50-ohm matching to the mixer and LNA ports in addition to some filtering. Some inter-stage filtering should be included in your circuit. You have to design your own filter based on your system requirement.

The transformer is for differential to single-ended conversion. You do not need it if you are are taking the output differentially.

Children
No Data