Post Go back to editing

MIXER AND LNA_OUT CONNECTION IN LT5500

What is the purpose of the LC circuitry connected at LNA_OUT pin and MIX_IN pin in the evaluation board in the datasheet? I want to connect the LNA_OUT to the MIX_IN. As described in the datasheet I need to connect an interstage filter between the two pins or I can use RC combination. CAn you provide me with more information about this filter or RC combination? 

Parents
  • FormerMember
    0 FormerMember
on Apr 15, 2019 1:15 PM

The LC circuit is for 50-ohm matching and filtering. Generally, an inter-stage filter should be used.  You can look up filter design in text books and on the internet.

Reply
  • FormerMember
    0 FormerMember
on Apr 15, 2019 1:15 PM

The LC circuit is for 50-ohm matching and filtering. Generally, an inter-stage filter should be used.  You can look up filter design in text books and on the internet.

Children
No Data