In PLL loop Filter Design , What is the role of VCOcap ?

In PLL loop Filter Design , What is the role of VCOcap ?

Parents
  • This capacitor may influence the frequency of the last pole of the loop filter. So if the design recommends 560 pF capacitance in the final stage, then if the VCO capacitance is 120 pF, this value should be subtracted from the final capacitance, to give a recommended cap value of 440 pF.

    For ADI VCO's, this tuning port capacitance is subtracted automatically from the final cap value.

Reply
  • This capacitor may influence the frequency of the last pole of the loop filter. So if the design recommends 560 pF capacitance in the final stage, then if the VCO capacitance is 120 pF, this value should be subtracted from the final capacitance, to give a recommended cap value of 440 pF.

    For ADI VCO's, this tuning port capacitance is subtracted automatically from the final cap value.

Children