AD8362 Front End Filter Help

Hi all,

I am designing a RF power detection circuit that is capable of detecting frequencies between 2.4GHz to 2.5GHz. I am keen to add a filter on the front end of the AD8362 and the component that I would like to use is the LFB182G by Murata. From their datasheet, it seems like their filter also acts as a balun so I will be using the RF power detector in differential mode. Is this component compatible with the AD8362? If so, do I still need to add DC blocking capacitors on the inputs (INHI, INLO)? Can you suggest a filter that is better suited? 


Many thanks!

Parents Reply Children