HMC641

Question on the HMC641 (we are using legacy HMC641LC4 parts), what is the typical, and the "minimum" & "maximum" digital control input current, for both I(INL) & I(INH)? How does the input maximum current rating vary as a function of the minimum & maximum V(INL) & V(INH) value range (-5V supply only)? Are these values also the limits in terms of the operating temperature range of the device since the typical input current rating is different between the devices?

Since the HMC641LC4 is legacy and the HMC641ALP4E is the current foundry part, what are the differences between the versions for the above questions? (Typical is specified for the HMC641ALP4E)