Post Go back to editing

IQ modulator and demodulator

Hi there,

We are looking for a pair of IQ modulator and de-modulator, which can be used as a loop back potential.

Looking at one of old threads below, it covers some of our questions. 

https://ez.analog.com/rf/f/q-a/72394/iq-modulators-and-iq-demodulator-1ghz-baseband-bandwith

We'd like to use evm  boards, of IQ demod adrf6820 or adrf6821 and IQ mod adrf6720 or adrf6720-27, together with DAQ2.

Our aim is to generate 500Mhz bandwidth RF signal while carrier frequency is not so important for now.

our question is that, is it possible to build a loop back mode use these IQ mod and demod evm boards?

Cheers,James

Parents
  • Hello,

    Yes, you can build a loop back system with those Mods and De-Mods. Those Mods and Demod themselves allow the wider 1dB baseband bandwidth than 500MHz. However, need to consider other roll-off over Frequency like RF output vs.Frequency(Figure 4 on ADRF6720) when you set carrier frequency.  Please refer to datasheet and user-guide to build with evm boards.

    Thanks

    Tony

  • Hi Tony,

    Many thanks for you reply and bringing roll off over frequency for adrd6720 to my attenation. 

    Over the holiday period, I also spotted a passive mixer, HMC8193, which is very interesting. Compared with above mods and de-mods, this IQ mixer only has all singled ended ports and becomes more attractive.

    It seems that using a pair of HMC8193, a RF loop back mode can be built, right?

    Say, here is my RF loop using mixer,  DAC-->MIXER(up) -->MIXER(down)-->ADC,

    1/  do I need a high/low pass filter in-between?

    2/ do I need low pass filter between DAC and MIXER up,?

    3/ do I need low pass filter between MIXER down and ADC?

    4/ Between mixer solution and mod/de-mod solution, which one is better?

    Regards,

    James

Reply
  • Hi Tony,

    Many thanks for you reply and bringing roll off over frequency for adrd6720 to my attenation. 

    Over the holiday period, I also spotted a passive mixer, HMC8193, which is very interesting. Compared with above mods and de-mods, this IQ mixer only has all singled ended ports and becomes more attractive.

    It seems that using a pair of HMC8193, a RF loop back mode can be built, right?

    Say, here is my RF loop using mixer,  DAC-->MIXER(up) -->MIXER(down)-->ADC,

    1/  do I need a high/low pass filter in-between?

    2/ do I need low pass filter between DAC and MIXER up,?

    3/ do I need low pass filter between MIXER down and ADC?

    4/ Between mixer solution and mod/de-mod solution, which one is better?

    Regards,

    James

Children