Hello,
I'm planning a DC coupled front-end for the AD9434 12-Bit ADC using the AD8352 Fully Differential Driver, as recommended in the datasheet and indicated in Fig. 43 in the AD9434 datasheet.
Since I will use the AD8352 in a single-ended to differential configuration with an input signal symmetric around GND, I am interested about the input voltage range when using
a) symmetric +-2.5V supplies
b) asymmetric +3V, -2V supplies
c) +5V, 0V supply
which I could not find in the corresponding datasheet
Is there a SPICE model available?
Thanks and regards
typo
[edited by: eti_ch at 5:35 PM (GMT 0) on 23 Dec 2018]