Post Go back to editing

Hmc453st89 amplifier

Hi...

I am designing a UHF/VHF circuit using the Hmc443st89 amplifier. The datasheet of the amplifier says in order to select the optimum performance, contact the application group.

I am designing the Amplifier at 436-438 MHz.

The datasheet doest not give any specific data at the above mentioned frequencies. The provided data is at 400 tO 410 MHz and then from 450 to 496 MHz.

It is requested to kindly provide the optimum performance circuit at 436 to 438 MHz. Further, any of the other graphs (vswr etc) of IC performance at these frequencies would also be really nice to have.

Parents Reply Children
No Data