Is it possible to use as "Vcco=+1.2V" ?
I can't find specification of input range for Vcci and Vcco.(It seems that "Vee" is required as fixed value "-2V".)
The condition of "Electrical Specification" in data sheet, it's all "Vcci=+3.3V, Vcco=0V, Vee=-3V, Vterm=0". However, I want to use as "Vcci=+3.3V, Vcco=+1.2V, Vee=-3V, Vterm=+1.2V" to adjust next interface level which similar to RSPECL. Data sheet also said as "RSPECL and RSECL Versions Available".So, I believe I can use as not only "Vcco=0V" but also such as "Vcco=+1.2V" or "Vcco=+2V".
However the concern of me, it is that there are no description of Vcco/Vcci input range except "Absolute Maximum Ratings" in data sheet.
Thanks,