parameter Reg00_1 = {7'd0,1'b0,8'h6C};//120MHz
parameter Reg01_2 = {7'd1,1'b0,8'h84};
parameter Reg02_3 = {7'd2,1'b0,8'h80};
parameter Reg03_4 = {7'd3,1'b0,8'h80};
parameter Reg04_5 = {7'd4,1'b0,8'h80};
parameter Reg05_6 = {7'd5,1'b0,8'h10};
parameter Reg06_7 = {7'd6,1'b0,8'h50};
parameter Reg07_8 = {7'd7,1'b0,8'h06};
parameter Reg08_9 = {7'd8,1'b0,8'h00};
The value of the emulation waveform and the register can be one pair. As long as the EN pin is pulled high, the mixer can work normally, but other performances remain unchanged by changing the value of the register. The peripheral pins of the mixer are also detected. And all are normal. But I don't understand why I can't control it. Please advise ~ Thank you