Hi,
We are planning to use your SP4T Switch part: HMC7992 for our frequency range of 4 to 5GHz where the maximum input power (rarely) expected is +29dBm (Avg) with PAR value of 6dB (Peak will be +35dBm) due to OFDM signal.
This input is connected only to RFC port so there is no chance of internal termination of this high power signal and switch will be always in through path, There is no Hot-switching at this above input power level.
1. Will it your switch withstand this input power level at +3.3V supply operation?
2. What is the Power handling of your switch if we operate the switch using +5V supply?
Regards,
Sugumar