Can anyone suggest mixer that suits for LO range of 2.4 - 3 GHz and IF frequency of 2 GHz ?

Hi,

I am looking for a mixer chip which should have LO range of 2 ~ 4 GHz and be able to output IF frequency of 2 GHz...

Actually, in the transmitter side, we are going to mix the LO signal (2 ~ 4 GHz) with AD9361 modulated output at IF frequency of 2 GHz. Hence, on the antenna side, we will get our desired band of transmission that is 4.4 ~ 5 GHz...

In the receiver side, we will do down tuning so that we will get IF frequency of 2 GHz...

Please suggest Mixers that suits for the above...

Thanks,

Muthu

Top Replies