Both the ADRF6520 and ADRF6518 have spectral noise density specified in dBV/Hz. It should be dBV/sqrt(Hz). The error has been noted (but not corrected) for the 6518. The same error cropped up in the 6520. It is correct for the ADRF6510 and ADRF6516.
ADRF6520
Recommended for New Designs
The ADRF6520 is a matched pair of fully differential low noise and low distortion programmable filters and variable gain amplifiers
(VGAs). Each channel...
Datasheet
ADRF6520 on Analog.com
ADRF6518
Obsolete
The ADRF6518 is a matched pair of fully differential low noise and low distortion programmable filters and variable gain amplifiers (VGAs). Each channel...
Datasheet
ADRF6518 on Analog.com
ADRF6510
Obsolete
The ADRF6510 is a matched pair of fully differential low noise and low distortion programmable filters and variable gain amplifiers (VGAs). Each channel...
Datasheet
ADRF6510 on Analog.com
ADRF6516
Obsolete
The ADRF6516 is a matched pair of fully differential, low noise and low distortion programmable filters and variable gain amplifiers (VGAs). Each channel...
Datasheet
ADRF6516 on Analog.com
Both the ADRF6520 and ADRF6518 have spectral noise density specified in dBV/Hz. It should be dBV/sqrt(Hz). The error has been noted (but not corrected) for the 6518. The same error cropped up in the 6520. It is correct for the ADRF6510 and ADRF6516.
Good catch.
I will add that to the list of changes to the next datasheet revisions of the ADRF6518 and ADRF6520.
Good catch.
I will add that to the list of changes to the next datasheet revisions of the ADRF6518 and ADRF6520.