The following Hittite VCOs from Analog Devices are now available in ADIsimPLL:
v1.1:
HMC507, HMC508, HMC509, HMC510, HMC511, HMC512, HMC513, HMC514, HMC515, HMC529, HMC530, HMC531, HMC534, HMC582, HMC583, HMC584, and HMC632.
Added in v2.0:
HMC391, HMC429, HMC430, HMC431, HMC466, HMC505, and HMC586.
v2.1: Bug fix.
Request additions in the comments below.
Installation instructions:
- Ensure ADIsimPLL v3.60.xx+ is installed and has been run at least once.
- Close any instances of ADIsimPLL.
- Download and extract the attached zip file.
- Copy the .lib file from the .zip file to the ADIsimPLL VCO library directory (top menu > Libraries > Explore Library Directory > VCO).
- Run ADIsimPLL. The added VCOs will now appear in the VCO Selection page of the ADIsimPLL wizard. See screenshot above.