problem in using ADRF6821 EVAL with the ACE

Hi,

I have a problem in using ADRF6821 EVAL with the ACE。

I connect  the EVAL board to PC by SDP-S, then start the ACE。

The screen shows up:

the software cannot detect the ADRF6821 EVAL even after installing the plug-in:

I installed the ACE software on Windows7 64bit 。

The DC current of the EVAL was 29 mA @5.6V ,while it should be about 40mA according to the user guides

It would be greatful if someone here could help me to fix this problem

Thanks. 

Joseph Jiang

    •  Analog Employees 
    on Sep 3, 2019 2:41 PM

    Hi Joseph,

    See attached for User Guide that includes guidance on SW installation.   Let me know if you have further questions.

    Thanks,

    Darrell

    PDF

  • Hi Darrell,

    I reinstalled the ACE software,and operated according to the Quick Start steps given by the User Guide:

    1, Connect the SDP-S controller board with the USB cable connected to the computer

    2, power up the ADRF6821- EVALZ

    3,  run the ACE software

    in step 3, the ACE cannot detect the ADRF6821 EVAL still, so I searched & installed the ADRF6821 package in Plug-in Marketplace,and repeated the step 1, 2, 3. The problem is still unresolved. It seems that the installed package doesn't match the EVALZ board?

    Thanks,

    Joseph