Article What are the THETAjc and THETAjb values (°C/W) for the MAX4003EUA, and how do they impact thermal performance?

The datasheet for the MAX4003EUA does not specify the THETAjc and THETAjb values. However, due to the low power consumption of the device (30 mW worst case), the thermal resistance values are not critical. Assuming a junction to case thermal resistance of 200 °C/W, the temperature difference from junction to board will be approximately 6 degrees. If the board temperature is 85 °C, the die temperature will be around 86 °C, well below the absolute maximum rating of 150 °C. Similarly, the junction to air thermal resistance is likely around 200 °C/W, resulting in a die temperature rise of at most 10 degrees above the air temperature. If a more conservative estimate is needed, a thermal resistance of 300 °C/W for both junction to case and junction to board can be used, which still results in a minimal temperature rise due to the low power consumption.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.