Article How do I synchronize MAX2880EVKIT to an external oscillator?

To synchronize MAX2880EVKIT to an external oscillator use the following procedure:
  1. Disconnect MAX2880EVKIT from all external sources.
  2. Remove the R24 resistor and JP2 jumper.
  3. Apply synchronization signal to the REFIN SMA connector
    • The synchronization signal must have a frequency between 10MHz to 100MHz / 210MHz (DBR=1 / DBR=0), and a peak-to-peak amplitude between 0.7V to Vcc 
    • The synchronization signal should be unipolar and should not be driven less than -0.3V below GND.
  4. Complete steps 2 to 10  in the MAX2880EVKIT quick start procedure.
    • The "REF. FREQ." box in the MAX2880EVKIT GUI should have the same values as the reference frequency being used. This will ensure all GUI parameters are properly calculated.

 

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.