When using the MAX2223, note that the VCO frequency is not the same as the LO frequency. For LO frequencies below 1125 MHz, the VCO runs at 4×LO due to a divide-by-4 output. For example, at 950 MHz LO…
KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the