Article Can VGG be tied to ground for biasing an MMIC amplifier, and what are the consequences if it is not possible to provide a negative gate voltage?

If VGG is tied to ground, the amplifier will not function correctly. Setting VGG to -2 V will put the amplifier in pinch-off mode, where no drain current flows and the amplifier is essentially turned off. Increasing VGG to a more positive value will decrease the drain to source resistance and increase the drain current. However, VGG cannot be set to 0 V as this will reduce the drain-to-source resistance to almost 0 V, causing the applied drain voltage to burn out the transistor. If a negative gate voltage cannot be provided, consider using a single positive supply voltage amplifier such as the ADL8100 or HMC8413.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.