ADL5801: FAQ

  • Created
  • Updated
Was this helpful?
  • ADL5801 Low Frequency Operation

    Q. The ADL5801 datasheet states that the device is capable of operation to frequencies as low as 10 MHz, yet the Typical Performance Characteristics plots only show data as low as 500 MHz. Is the device…
  • ADL5801 Mixer Performance when driven single-ended on both its RF and LO ports

    Q. How does ADL5801 active mixer perform when driven single-ended on both its RF and LO ports without baluns? In some applications, baluns/transformers are not preferred, due to certain requirements…
  • ADL5801: s-parameter

    Question Do you have the s parameters of ADL5801? Answer Please see attached s parameters file.
  • ADL5801: specification at 4GHz

    Question I am using ADL5801 in the frequency band from 4400MHz to 4600MHz. Therefore, I want to get some details of ADL5801 working in the band such as input IP3, which do not be shown in the datasheet…
  • ADL5801-EVALZ Evaluation user guide doc missing

    Question No user guides are included in the eval-board kit. Nor can I find any user guide for the ADL5801-EVALZ in the website product page. Therefore unsure of how to power it up. Answer The ADL5801…
  • S-Parameters for ADL5801 Mixer

    Question I'm developing a wideband RF measurement system employing the ADL5801 mixer and need to optimize the RF Port input return loss for the frequency range of 1.5 to 3.0 GHz. Therefore it would…
  • Threshold voltage to disable the ADL5801/2

    Q. What is the threshold voltage to disable to the ADL5801/2 mixer? ------------------------------------------------------------------------------------------------------------------------------ ---…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.