ADF4360-7: FAQ

  • Created
  • Updated
Was this helpful?
  • ADF4360-7: ADIsimPLL gets small L value

    Question I have a question about ADIsimPLL for simulating ADF4360-7. When I am setting the output as a fixed frequency of 818.4MHz, PFD=2.5575, the external inductor L1=L2=611pH. But we can not get…
  • ADF4360-7_output impedance-2

    Question In ADF4360-7's datasheet, it says: "Experiments have shown that the circuit shown in Figure 30 provides an excellent match to 50 Ω over a limited operating range of the ADF4360-7 (850 MHz…
  • ADF4360-7_VCO Open Loop Phase Noise Test

    Question I am using ADF4360-7. Here the VCO Phase-Noise is measured in Open-loop conditions. How do I configure the EVB as open-loop? Answer Open loop test need to program CP to 3-state and apply a very…
  • What is the storage temperature range for the ADF4360-7?

    While there is no storage temperature spec for ADF4360-7 in its datasheet, I did find that the datasheets for two other family members, ADF4360-8 and ADF4360-9 indicate a storage temperature of -65 degC…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.