Article ADF4360-5: Reference I/P signal

Question

We are driving the reference input of the device with a AD8170.
The output of the AD8170 is a 66MHz square wave with a slew rate of 600V/uSec,
1.2Vp-p.
Is this signal applicable with the ADF4360-5 device?

Answer

The REFIN input is a CMOS logic input, so therefore, you can either AC couple a
min signal level of 0.7volts or DC couple a TTL/CMOS square wave input signal.
In your case, you could AC couple your input signal.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.