AD8364: FAQ

  • Created
  • Updated
Was this helpful?
  • AD8364 Operation at 2.7 GHz

    Question: AD8364 is specified to operate up to 2.7 GHz but the datasheet only shows data at 2.5 GHz. Do you have any data showing performance up to 2.7 GHz. Answer: The attached plots show sweeps of…
  • Calculating VSWR using dual Linear-in-dB RMS Detector

    Q uestion : If I’m using a device such as AD8364 or HMC1030 to measure VSWR, how do I actually get from output voltage (or ADC code) to VSWR? Answer : The short answer is that the return loss in dB…
  • Frequency Dependent Power Measurement Error

    Question We are using the AD8364 in the band 2.110 to 2.155GHz. We are getting a relatively large frequency dependent power measurement error. For example, if the device is calibrated (intercept and slope…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.