AD8302: FAQ

  • Created
  • Updated
Was this helpful?
  • AD8302 evaluation board information

    Question Does any information about the eval board AD8302-EVALZ exist? Beside the Gerber Files. Answer You should find a lot of eval board stuff on page 21 of the AD8302 datasheet rev. A. Also, attached…
  • AD8302 Full phase detection

    Question I have purchased an AD8302 evaluation board and am looking to use it to detect a phase difference of the incoming signals. Is it possible to tell the difference between a positive and negative…
  • AD8302 Gain and Phase with no Input Signal

    Q. What is the output voltage of the AD8302 gain/phase detector when there are no signals present on the inputs? --------------------------------------------------------------------------- A. …
  • AD8302 Gain/Phase Detector, Response to Modulated Signals

    Q. How does the AD8302 gain/phase detector respond when it is driven by signals such as a modulated carrier whose phase is changing continuously? ------------------------------------------------…
  • AD8302 Gain/Phase Detector: Operation as a Frequency Discriminator

    Q. Can the AD8302 gain/phase detector be used as a frequency discriminator? ----------------------------------------------------------------------------------------------------------------- A.…
  • AD8302 spice model and gerbers for eval board

    Question AD8302 spice model and gerbers for eval board: Do you provide details suitable for "Proteus/ISIS7 professional pcb package", including a spice model which can be used for simulations ? If…
  • AD8302's Small Signal Envelope Bandwidth

    Question I am not sure about "Small Signal Envelope Bandwidth" mentioned in the section of SPECIFICATIONS. Would you please help explain below parameter? Answer the small signal bandwidth is essentially…
  • AD8302: Hot to measure +/- 180deg phase

    Question I am interested in a build a Vector Network Analyzer but AD8302 can only detect +-90 degrees. To make a good Vector Network Analyzer its not necessary to detect +-180 degrees? Answer IN fact…
  • AD8302: Offsetting the phase output

    Question With AD8302, is there a simple circuit layout that lets me offset phase detection response? For example, I'd like to have maximum value, 1.8V, when phase difference is -45 degrees, avoiding…
  • AD8302: VPHS output changes with different input signal amplitude

    Question There is a question about AD8302 as below. I connect the node 1 and node 2 with VINA and VINB as below. When I changed the amplitude of input signal V1, the output of VPHS will change too…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.