Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
      New KCC Quiz AQQ299 about Opamp open looop gain and LTspice (a kind proposal from Al Butvidas)

      1. Quote of the month: " A good friend calls you in jail. A great friend bails you out of jail. Your best friend sits next to you and says 'wasn't that...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Understanding Voltage Domain Isolation in Field-Bus...
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
    Master FPGA-Based DSP Design: The Complete Building Blocks Guide You Need to Read

    The Engineering Mind Blog on EngineerZone presents an exceptional five-part series titled " DSP Building Blocks " that walks engineers through the essential...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    PSM Integration for Enhanced Module Solutions in 48 V Data Centers

    The integration of the LTC2971 into quarter brick solutions for 48 V data centers enhances monitoring, control, and reliability by providing high precision...

EngineerZone
EngineerZone
Reference Designs
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Reference Designs
Reference Designs
Documents CN0269: FAQ
  • Forums
  • File Uploads
  • Docs/FAQs
  • Members
  • Tags
  • Cancel
  • Documents
  • +CN-0172: FAQ
  • +CN-0189: FAQ
  • +CN-0196: FAQ
  • +CN-0267: FAQ
  • CN0269: FAQ
  • CN0273: FAQ
  • +CN-285: FAQ
  • +CN-0287: FAQ
  • CN0319: FAQ
  • CN0326: FAQ
  • CN0332: FAQ

CN0269: FAQ

Q:

Hello,

I've looked through the CN0269 schematics for the pinout for J6 (a 2x6 0.1 header).  This appears in the gerbers (from .zip archive) but not in either the .pdf schematic or the PADS .sch logic. From the gerbers, it appears that this header (J6) might be connected to the DOT SPI lines.  Any help would be appreciated.

Bob.


A:

Hello Sir

Thanks a lot for your help to points out this issue. I would update the design support package as soon as possible.

Thank you for your interest in this circuit.

My pleasure to answer your question and help to solve your question.

Willie.


A:

Hello Sir

The design package is updated on website. Please downloaded from the link below:

http://www.analog.com/en/circuits-from-the-lab/CN0269/vc.html

Sorry for the inconvenience.

Wish you all the best.

Willie.


Q:

hello

why there are two digital and analog GND joint point?  (Such as P4 and P5) And they are not in top or bottom layer,.Is it a mistake?

THANKS


A:

Hello Sir

In order to provide a short current back-path for ADC digital interface, we usually put a 0ohm resistor or the GND joint point, as used in this circuit, just under or near the ADC digital interface. The same way of thinking, Analog-Multiplexer has digital control logic as well as analog path just like the ADC. When driving the multiplexer switching with fast digital signal, we need to provide a short back path for the driving current near the multiplexer.

With best regards,

Willie

Q:

hello

thanks for your answer

but base your words I have some other questions:

such as if only one channel is sampled(no switch),in this situation two GND joint point is not a good way. So I must make my system always in a switch mode?

THANKS


A:

Hello Sir

Yes, you can only add one GND joint when your system never switching Multiplexer at high frequency but if your circuit need to scan all the channel one by one to realize the multi-channel DAQ system, you could follow the way CN0269 did. But to be honest, both way could work and without a big difference and the difference is hard to find out and usually ignorable.

Tags: cn0269