Accelerate RF Subsystem Integration with COTS SoMs and Phased Array Solutions. As building a subsystem from early prototype to full deployment is never...
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
      1. Quote of the month: " Friendship is like money - easier made than kept " - Samuel Butler 2. New quiz AQQ300 about a divisibility by 6 puzzle ...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Taming the AI Power Storm: Part 2 of 3 Test your...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Calibration Implementation Techniques for Multichannel Phased Array Subsystems

    Learn about phase-calibration techniques used for characterizing a 16 transmit and 16 receive X-band phased array subsystem based on a mixed-signal front...

EngineerZone
EngineerZone
Reference Designs
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Reference Designs
Reference Designs
Documents CN0319: FAQ
  • Forums
  • File Uploads
  • Docs/FAQs
  • Members
  • Tags
  • Cancel
  • Documents
  • +CN-0172: FAQ
  • +CN-0189: FAQ
  • +CN-0196: FAQ
  • +CN-0267: FAQ
  • CN0269: FAQ
  • CN0273: FAQ
  • +CN-285: FAQ
  • +CN-0287: FAQ
  • CN0319: FAQ
  • CN0326: FAQ
  • CN0332: FAQ

CN0319: FAQ

Q: 

I have a problem with CN0391 EVAL Board, can you please point me how to solve it?

CN0319 EVAL Board have a button(SD) connected to P2.2 Pin on ADuCM360 MCU. But this pin is only GPIO without IRQ. can you please let me know how can i handle when SD button is pressed?

Thanks !

A:
The pin 2.2 on the ADuCM360 functions as a bootloader pin, on the EVAL-CN0319-EB1Z.  This will allow you to download a hex file using the windows serial downloader tool from the MCU team here at ADI.  That is the primary function for this button and pin on the EVAL-CN0319-EB1Z.

Brandon

Q:
Hi   

Thank for your information ! So, is there any way to handle this button?

I want to test some example code comes with CN0319 EVAL board. But, some of examples using external interrupt(IRQ4).

And, can you please show me more information about Windows Serial Download ?

Thanks !

A:


The Windows Serial Downloader is an application that will program/flash the MCU without the need of a programmer/debugger like Segger.

I'm not sure I understand what you mean by "handle the button"?  IRQ4 is on port 1.1 which is pin 39, and has nothing to do with the bootmode pin 2.2

Brandon.

Tags: cn0319