Post Go back to editing

LB3031A Injection Transformer

Thread Summary

The user inquired about the frequency characteristics of the LB3031A Injection Transformer at a 5° phase difference, the model number of the OPA driving it, and the OPAs used in DA1, DA2, and DA3. The final answer stated that the design details of the LTpowerAnalyzer, including part-specific model numbers and performance data, are confidential and not being disclosed. No specific technical parameters or workarounds were provided.
AI Generated Content

If possible, please answer the following questions.
1: What are the frequency characteristics of the LB3031A Injection Transformer when the phase difference is 5°?
2: What is the model number of the OPA driving the Injection Transformer?
3: What are the model numbers of the OPAs used in DA1, DA2, and DA3?
I would like to measure the loop gain using ADALM2000+Scopy.
Thank you in advance for your cooperation.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.