Post Go back to editing

Inquiry Regarding LTPA Impedance Data Conversion to S-Parameter

Thread Summary

The user inquired about converting LTpowerAnalyzer impedance analysis data to S-parameter format for Power Distribution Network and Power Integrity simulations. The final answer explains that LTpowerAnalyzer only provides Z22 (output impedance) data, and converting to S-parameters requires a full Z-parameter set. No direct S-parameter measurement or export capability is available in LTpowerAnalyzer. The user can refer to a literature source for Z-to-S parameter conversion methods.
AI Generated Content
Category: Software
Product Number: LTpowerAnalyzer
Software Version: 1.9.0.0

Hi Team,

I have a question regarding the LTpowerAnalyzer impedance analysis feature.

Is there any method to convert the impedance analysis data from LTPA into an S-parameter format?

We would like to perform Power Distribution Network and Power Integrity simulations based on S-parameter data.

Although Scopy does not appear to support this functionality, I believe the frequency-impedance data from LTPA could potentially be used to derive S-parameters.

  • Ideally, it would be very helpful if the data could be exported directly as a Touchstone (.s1p) file.

The converted S-parameter data would be used during post-layout (post-simulation) analysis, after PCB artwork completion or in progress, for SoC-level PI evaluation.

While there is no immediate demand, we anticipate this capability will become essential in upcoming customer projects.

Therefore, if it’s possible to extract S-parameter data of a Power IC using an EVM and LTPA, it would be extremely beneficial for customer PI analysis and design validation.

Best regards,
Alexander

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.