Post Go back to editing

CN-0099

The circuit below is basically taken from CN-0099 and is part of a weight cell :

Our problem is that on one of our weight cell units has failed because the ADA4096-2 op amp was broken.

( We use ADA4096-2 instead of the op amp AD8603 suggested in CN-0099 to allow +24V circuit operation).

Measurements with the broken ADA4096-2 (with a 500ohm Rload attached between 4-20mA and 0V):

+IN @ U3.3 was measured to 496mV

SENSE @ U3.5 was measured to 5.996V

REF @ U3.1 was measured to 5.5V 

Also the 4-20mA output @ U7.3 was measured to 5.5V across 500ohm Rload.

So, the output 4-20mA output current was actually as much as 11mA (5.5V / 500ohm) even though the current through the 124ohm shunt resistor was only 4mA. Calculation: (5.996-5.5V) / 124ohm. This meant that U7.3 was sourcing 11mA - 4mA = 7mA to the 500ohm Rload.

Measurements after replacing the broken ADA4096-2:

+IN @ U3.3 was measured to 496mV

SENSE @ U3.5 was measured to 2.496V

REF @ U3.1 was measured to 2V 

The 4-20mA output @ U7.3 was now measured to 2V across 500 ohm which is correct for 4mA.

We need help to understand why the ADA4096-2 op amp in this case have failed in our weight cell application.

Parents
  • Hi Harry,

    Before we proceed posting a formal FA:

    1. Do you think ADA4096-2 is a suitable op amp for replacing AD8603 in our +24V single supply application ?

     

    2. Do you think lack of ESD transient protection in the circuit above is a "probable cause" for ADA4096-2 failure ?

     

    According to datasheet ADA4096-2 input pins have internal overvoltage protection up to 32 V above and below the supply rails. But I guess this still make them vulnerable to ESD transients.

    If your is yes on my questions 1 and 2 above, we simply need to add some transient protection to our circuit.

    Rgds, Tore Kallevik

Reply
  • Hi Harry,

    Before we proceed posting a formal FA:

    1. Do you think ADA4096-2 is a suitable op amp for replacing AD8603 in our +24V single supply application ?

     

    2. Do you think lack of ESD transient protection in the circuit above is a "probable cause" for ADA4096-2 failure ?

     

    According to datasheet ADA4096-2 input pins have internal overvoltage protection up to 32 V above and below the supply rails. But I guess this still make them vulnerable to ESD transients.

    If your is yes on my questions 1 and 2 above, we simply need to add some transient protection to our circuit.

    Rgds, Tore Kallevik

Children