Post Go back to editing

DEMO-AD5700D2Z HART_CLK connection

Hi,

This is regarding DEMO-AD5700D2Z board. I just started programming and evaluate the performance of the ICs in-order to zero in on them. I see that HART_CLK is connected to both P2.0 and P1.0. Can someone please explain me what is the reason to connect to two pins?

Also, on a custom board, I want to connect HART_CLK to just P1.0 as I want to use P2.0 and P2.1 as I2C lines. Is it feasible?

Thanks,

Spoorthy

ad5700 ad5700-1 hart demo-ad5700d2z

Parents Reply Children
No Data