Post Go back to editing

DEMO-AD5700D2Z HART_CLK connection

Hi,

This is regarding DEMO-AD5700D2Z board. I just started programming and evaluate the performance of the ICs in-order to zero in on them. I see that HART_CLK is connected to both P2.0 and P1.0. Can someone please explain me what is the reason to connect to two pins?

Also, on a custom board, I want to connect HART_CLK to just P1.0 as I want to use P2.0 and P2.1 as I2C lines. Is it feasible?

Thanks,

Spoorthy

ad5700 ad5700-1 hart demo-ad5700d2z

Parents
  • Hi Spoorthy,

    On the ADuCM360 microcontroller, P2.2 is dedicated to initialize UART download mode(held low during reset). You can not transfer this function to another pin. You have the option to not use the UART download mode. There is also dedicated serial wire/JTAG download and debug using pins 47 and 48.

    Please refer to ADuCM360 datasheet and user guide for more information:

    Datasheet

    User Guide

    Thanks

    JB

Reply
  • Hi Spoorthy,

    On the ADuCM360 microcontroller, P2.2 is dedicated to initialize UART download mode(held low during reset). You can not transfer this function to another pin. You have the option to not use the UART download mode. There is also dedicated serial wire/JTAG download and debug using pins 47 and 48.

    Please refer to ADuCM360 datasheet and user guide for more information:

    Datasheet

    User Guide

    Thanks

    JB

Children
No Data