Post Go back to editing

DEMO-AD5700D2Z HART_CLK connection

Hi,

This is regarding DEMO-AD5700D2Z board. I just started programming and evaluate the performance of the ICs in-order to zero in on them. I see that HART_CLK is connected to both P2.0 and P1.0. Can someone please explain me what is the reason to connect to two pins?

Also, on a custom board, I want to connect HART_CLK to just P1.0 as I want to use P2.0 and P2.1 as I2C lines. Is it feasible?

Thanks,

Spoorthy

ad5700 ad5700-1 hart demo-ad5700d2z

Parents
  • Hi JB.Chua,

    Thanks for the reply.

    I'm sorry but I had to add another query. P2.2 is used for download push button. On a custom board, can I use P1.3 for download push button? (in order to use P2.1 as SDA line)

    Would I still be able to download code via CM3WSD?

    Thanks,

    Spoorthy

Reply
  • Hi JB.Chua,

    Thanks for the reply.

    I'm sorry but I had to add another query. P2.2 is used for download push button. On a custom board, can I use P1.3 for download push button? (in order to use P2.1 as SDA line)

    Would I still be able to download code via CM3WSD?

    Thanks,

    Spoorthy

Children
No Data