Post Go back to editing

CN0565 Reference Design – ADM7150 VREG Pin Connected Directly to VIN

Category: Hardware
Product Number: EVAL-CN0565-ARDZ

Hello ADI Engineering Team,

I am currently studying the EVAL-CN0565-ARDZ reference design and developing a custom PCB based on this design.

I noticed that the ADM7150ARDZ-3.3 (U5) has its VREG (Pin 1) directly connected to VIN (Pin 8) and the +5 V supply.

I have verified this connection in the published schematic, the IPC-356 PCB netlist, and photographs of the actual evaluation board.

However, according to the ADM7150 datasheet, VREG should be bypassed to ground with a 10 µF or greater capacitor. The typical application circuit shows VREG and VIN as separate nodes.

I would appreciate clarification on the following questions:

  1. Is the direct connection between VREG and VIN intentional in the CN0565 reference design?

  2. If intentional, what is the technical reason for this configuration? Does it affect the regulator's noise performance, PSRR, or stability?

  3. For a new PCB based on CN0565, would ADI recommend retaining this connection or following the ADM7150 datasheet's typical application circuit?

Thank you for your time and assistance.

Best regards

  • Hi  ,

    No, this is not intentional. It’s good that you caught this, as it was an error introduced during the ADM7150 symbol update. Shorting the VREG and VIN pins bypasses the intended VREG filtering and can compromise the ADM7150’s PSRR and stability performance. For new PCB designs, we recommend following the typical application circuit in the ADM7150 datasheet to achieve the best possible performance.

    Best Regards,
    Michelle

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.