Hello Analog Devices support team,
I am currently integrating the CN0359 conductivity measurement system into my own project. The measurement performance is correct and the conductivity readings are as expected. However, I am facing an issue with power consumption and component temperature.
In my implementation, the total system current consumption is around 150 mA, and most of this power consumption comes from the EC sensor excitation circuit. The analog circuitry, including the ADA4627 and AD8253 amplifiers, is powered from a ±15 V supply.
Although the system operates correctly and the measurement results are accurate, the ADA4627 and AD8253 amplifiers become noticeably warm during operation. I would like to understand whether this temperature rise is expected in the CN0359 configuration or if there are any design improvements that can reduce the power dissipation.
Could you please advise on the following points?
- What are the typical power dissipation and expected temperature rise values for the ADA4627 and AD8253 when operating from ±15 V supplies in this application?
- Are there any recommended circuit modifications, PCB layout improvements, or thermal considerations to reduce the heating of these components?
- Are there lower-power or lower-temperature alternatives for ADA4627 and/or AD8253 that can provide similar measurement performance?
- Is there any recommended method to reduce the overall power consumption of the EC sensor excitation stage while maintaining measurement accuracy?
For reference, I am using the CN0359 architecture with ±15 V analog supplies. The system operates correctly and provides accurate conductivity measurements, but the power consumption and thermal performance are higher than expected.
Thank you for your support.
Best regards,