Post Go back to editing

Information about the evaluation board

Category: Hardware
Product Number: EVAL-CN0350-PMDZ

I purchased a EVAL-CN0350-PMDZ evaluation board, i want a few clarifications about the board which are defined as follows:

1. I want a complete schematic diagram of the EVAL-CN0350-PMDZ board, other than which is given in circuit note CN-0350.

2. I am using 1510A precision signal generator for generating charge signals which is used for giving input to the board. Now, i want to know the expected input (charge) and output (voltage) relation for the board so that i can verify it by giving suitable input charge signals.

3. I also want to know the minimum value of AC charge signals which is supported by the board for conversion to voltage.

Thread Notes

Parents
  • Hi  ,

    Please see the schematic and answers below. Let me know if this works for you.

    1. I have attached a copy of the Schematic for EVAL-CN0350-PMDZ
      02-047068-01-a-1.pdf
    2. The CN‑0350 signal chain consists of a charge amplifier stage (U1A with feedback capacitor C2) followed by a non‑inverting gain stage (U1D, set by R7 and R8), with both stages referenced to a mid‑scale offset voltage V_HREF of 1.25 V. The charge injected at the summing node is integrated onto C2 and then scaled by the second stage, giving the overall transfer function:

       ​​

      When you drive the board through the CAL input (TP1–TP2) using your 1510A precision signal generator, the injected charge is defined by:

      ​

      where C_CAL is the calibration capacitor in series with the 1510A output. Substituting this in, the end‑to‑end relationship becomes:

       ​

      Using the default board values (C2 = 1 nF, C_CAL = 1 nF, R8 = DNP giving unity gain), a ±1 V peak signal from the 1510A injects ±1000 pC of charge and produces an ADC output swing between 0.25 V and 2.25 V centered around 1.25 V, which matches the calibration result shown in Figure 4 of the circuit note. Please also ensure that the 1510A output is floating (isolated) with respect to the board ground, since the CAL input sits at the 1.25 V HREF common‑mode level.

    3. There are two limits to consider — one in amplitude and one in frequency. On the amplitude side, the smallest resolvable charge is set by the 12‑bit AD7091R ADC's 1 LSB step, given by:

      Referred back to the input through the charge amplifier:

      at the default unity gain with C2 = 1 nF. Accounting for AD8608 noise and offset contributions, a reliably distinguishable AC charge is on the order of a few pC peak. On the frequency side, the low‑frequency corner of the charge amplifier is set by R3 in parallel with C2:

      with the default R3 = 100 MΩ and C2 = 1 nF — so AC signals below roughly 1.6 Hz will be attenuated by the DC feedback path and should be avoided. For best results during your verification, I would recommend keeping the test frequency in the flat region between approximately 10 Hz and 100 kHz (the circuit note itself uses 1 kHz for calibration), which keeps you well inside both the low‑ and high‑frequency corners of the design.

    Regards,
    Michelle

  • Hi  !

    Do you still need any assistance?

    Regards, Elena

Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.