Description: Hello, I am working with the CN0565 platform along with the ADICUP3029 board. I am facing an issue while trying to program the CN0565 firmware: When I copy the provided HEX file to the DAPLINK drive, a FAIL.TXT file is generated. The content indicates that the interface firmware failed to reset/halt the target MCU. Using pyOCD (pyocd list), the probe is detected but the target shows as "n/a". Using libiio (iio_info), only the local backend is visible and no USB/IIO device corresponding to CN0565 appears. Steps already attempted: Rebuilt and installed latest libiio from source Tried flashing firmware multiple times (including reset during drag-and-drop) Verified USB connection and cable Tested on Linux environment (Ubuntu 24.04) Current behavior: DAPLink drive mounts correctly Firmware flashing fails consistently with FAIL.TXT Target MCU is not detected over SWD Could you please help identify: Whether this indicates a firmware issue or a connection/power configuration issue Any required jumper/switch settings for proper operation Recommended recovery steps for the ADICUP3029 in this condition Any guidance or known issues related to CN0565 initial setup would be helpful. Thank you.