Hello,
My final goal is measure is impedance and EIS, and for now it is not even possible to setup a simple read.
I am trying to communicate the EVAL-AD594-ELCZ shield directly from a Raspberry Pi 5 via SPI, without the ADICUP3029 to try to get impedance data. I tried with ADICUP3029 I could not get output data even I tried for days.
My problems:
Reading ADIID register (0x0400) always returns 0x80 on every byte regardless of SPI mode (0,1,2,3), speed (200kHz-1MHz), or library used (spidev, python-periphery). I tried to remove the MISO (DS12) wire gives 0x00, confirming the board is driving MISO but stuck at 0x80.
1. Are there known SPI compatibility issues with Raspberry Pi 5?
2. Is 0x80 a known error state for the AD5941 SPI interface?
3. Does the AD5941 require firmware initialization before responding to external SPI?
Thanks in advance :) !