Post Go back to editing

Reset (hardware and software) BatImpedance

Thread Summary

The user inquires about initiating EIS measurements on a lithium-ion cell using the BatImpedance software from the AD5940-examples repository via a software reset instead of a button press. The final answer suggests checking ad5940.c for available reset functions. No specific function is mentioned, and no additional clarifications are provided.
AI Generated Content
Category: Hardware
Product Number: EVAL-AD5941BATZ, AD5941, AD5941

I am using the BatImpedance software from github.com/.../ad5940-examples.
Currently, I start the EIS measurement of an ion lithium cell by pressing a button on the CN-0510 target board.
Would it be possible to initiate the programme via a software reset? If so, which function should I use?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.