Post Go back to editing

Measuring 6 cells of a battery pack with CN0510 by multiplexing

Thread Summary

The user is experiencing poor EIS measurement results when using force cables on the main terminals of a 6-series battery pack with the AD5941. The final answer suggests that the AC current excitation across a larger impedance in the main terminal configuration can cause deviation from Ohm's law due to non-linearity. The user should adjust the DC bias for each cell and ensure the ADC input range is within +900mV to -900mV. The accompanying answers recommend checking the gain of the input potential and adjusting the ADC PGA gain and RTIA values.
AI Generated Content
Category: Hardware
Product Number: CN0510

Hello, I have an 6 series battery pack. I want to perform EIS test on each cell by multiplexing the AD5941. So for sense cables AC coupler - Buffer - Multiplexer looks like the correct way. I am confused about the force cables, should I mux those also? or may I do the excitation by the main terminals of the battery pack?

When I tried the force cables on the mains and switching the sense cables of cells on CN0510 my measurement results gets worse. Is there a way to make this configuration work. I use sensorpal for the measurements right now but when i develop the card i will use custom software.

Parents Reply Children
  • The difference between the two configurations is that

    - AC current excitation appears across a larger impedance in T2T case versus smaller impedance in differential case.

       There could be deviation from Ohms law in 1st case due to non-linearity at higher impedance.

    - EXC_P(see CN0510 schematic) DC value is changed

    Behavior of T1B31BG (Darlington pair) in CN0510:

    You may change the DC Bias for each case and check.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.