Post Go back to editing

Measuring 6 cells of a battery pack with CN0510 by multiplexing

Thread Summary

The user is experiencing poor EIS measurement results when using force cables on the main terminals of a 6-series battery pack with the AD5941. The final answer suggests that the AC current excitation across a larger impedance in the main terminal configuration can cause deviation from Ohm's law due to non-linearity. The user should adjust the DC bias for each cell and ensure the ADC input range is within +900mV to -900mV. The accompanying answers recommend checking the gain of the input potential and adjusting the ADC PGA gain and RTIA values.
AI Generated Content
Category: Hardware
Product Number: CN0510

Hello, I have an 6 series battery pack. I want to perform EIS test on each cell by multiplexing the AD5941. So for sense cables AC coupler - Buffer - Multiplexer looks like the correct way. I am confused about the force cables, should I mux those also? or may I do the excitation by the main terminals of the battery pack?

When I tried the force cables on the mains and switching the sense cables of cells on CN0510 my measurement results gets worse. Is there a way to make this configuration work. I use sensorpal for the measurements right now but when i develop the card i will use custom software.

Parents
  • Hi,

      Excitation can be given at the main terminals alone.

      The AC potential across each battery is measured by ADC of AD5941.

      If this potential is very small or very big (outside allowed voltage input range of ADC), results will be erratic due to ADC saturation.

      You may adjust the gain of input potential

    - by opamp stages or bypassing them as shown in CN0510 schematic below:

    or by changing ADC PGA gain and RTIA values inside device via code.

  • Hello Akila,

    Thank you for your answer. There is an example measurement on one of the series of my battery pack. when I connect all the cables on the first series the result looks expected and it is consistent, but when I connect the F cables on the main terminals of the battery pack the results is as you see in the graph, it drifts from the reference measurement a lot. I have already checked that AIN2 and AIN3 (from the R17 and R20) signals are within +900mV -900mV. How can i make this result better? What should i modify on CN0510? What could be the reason of this deviation? (the example measurement is performed on cn0510 with the parameters of DC Bias: 1200mV, AC amplitude: 600mV, Frequency: 1Hz-1kHz, Points: 30)

    Thank you.

  • Hi,

     Could you please show your connection with block diagram for clarity?

Reply Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.