Post Go back to editing

Waiting for transfer from controller - CN0276 + CB1Z

Thread Summary

The user is missing the 'SDP EEPROM Programmer software' and 'CN0276 Programming File' for the EVAL-CN0276-SDPZ board. The final answer suggests using the AD2S1210 chip with the latest Kuiper Linux for Raspberry Pi, adding 'dtoverlay=ad2s1210-overlay' to the config.txt file, and using the IIO Oscilloscope for control. An archived SDP EEPROM Programmer was provided, and the user confirmed it worked on a different Windows 10 device. The engineer is also exploring the possibility of a custom API for interaction with the board.
AI Generated Content
Category: Software
Product Number: Waiting

I have EVAL-CN0276-SDPZ + EVAL-SDP-CB1Z but the download CN0276_Evaluation_Software doesn’t contain the ‘SDP EEPROM Programmer software’ or the ‘CN0276 Programming File’ mentioned here.
That page literally lists those two items as “Supplied with CD" but the package of the EVAL-CN0276-SDPZ doesn't include it.

Can I download those files from another site?

Please help,

Thank you.

Parents Reply Children
  • Hi Julian,

    The CN0276 board primarily uses the AD2S1210 chip, which is supported by a Linux driver included in the latest version of Kuiper Linux for Raspberry Pi.

    I’ve attached the schematic diagram for your reference. You can use the JTAG header (J2) to interface the CN0276 with the Raspberry Pi (just make sure to set SOE pin low to activate the internal SPI interface). Alternatively, you may use the ADZS-BRKOUT-EX3 board to connect via the FFC/FPC port.

    Here’s the link to download the Kuiper Linux image:

    Analog Devices Kuiper Linux [Analog Devices Wiki]

    Schematic Diagram:

    To enable the system driver, please add the following line to the configuration file, directly below the [all] section, you can find the config.txt file on the /boot/ folder:

    dtoverlay=ad2s1210-overlay
    

    After adding this line, restart the system to apply the changes.

    Once the system is up, you can verify if the device is detected by running:

    iio_info
    

    If the device appears in the output, you can then use the built-in IIO Oscilloscope for control and visualization through its GUI.

    Let me know if you need further assistance with the setup or testing.

    Regards,

    Pao

  • Hello Pao,

    That's a very useful information. I have a spare Raspberry Pi 4B, so I'll try with it.

    Best Regards,

    Julián

  • Hi Julián,

    Just checking in, how’s it going with the CN0276 setup on your Raspberry Pi 4B?

    Let me know if you need any assistance.

    Best Regards,
    Pao

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.