Hi,
I’m considering interfacing the CN0566 with an SDR solution other than the PlutoSDR. I’ve reviewed the PlutoSDR HDL and schematic, and I believe I understand the GPIO connections required.
I have two questions to better understand the design:
1. While going through the CN0566 schematic, I noticed the SPI signals (SDIO, SDO, SCLK, CSB0, CSB1, CSB2) are not routed to the 14-pin socket. Could you clarify whether the PlutoSDR actually provides this SPI interface to the board? If so, is it implemented through the axi_quad_spi interface in the HDL? Additionally, how are the CSBx signals intended to be routed? I've attached part of the schematic I'm referring to.
2. Is there any way to make the CN0566 board tolerant to 3.3 V CMOS levels when interfacing with an SDR device?
Thanks in advance for your help.