Post Go back to editing

CN0565+ADICUP3029 : no device found

Thread Summary

The user encountered a 'Serial Connection Error! No device found' when running example scripts for EVAL-CN0565-ARDZ and using IIO Oscilloscope. The issue was resolved by uploading the hex file and ensuring the correct baud rate (230400) and switch settings (S2 to USB, S5 to WALL/USB). The problem was ultimately due to a faulty ADICUP3029, which was replaced.
AI Generated Content
Category: Hardware
Product Number: CN0565

I configured the environment according to the EVAL-CN0565-ARDZ User Guide, and I got an error when running cn0565_example_single.py or main.py:Serial Connection Error! No device found


I modified the port or baud rate, but it didn't work.

And I also use the iio oscilloscope , and it also can't connnect.

I use the iio-info get the Unable to create Local IIO context

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.