Hello! I am measuring the impedance of a 21700 NCA battery using the EVAL-AD4591BATZ. I'm collecting data using Sensorpal and plotting it through Python. The graph is a sweep from 1Hz to 50000Hz. I'm not sure if the graph looks correct. If it is correct, I'm curious if the imaginary axis is corrected to negative values
.
. Also, no matter which battery I connect, the real component (Rs) is always the same at 0. I'm attaching the Python plot graph Thank you