Post Go back to editing

CN0359

Thread Summary

The user encountered issues with the EVAL-CN0359-EB1Z Rev. A evaluation board not working after compiling and loading the ADuCM360_demo_cn0359_reva project in CrossCore Embedded Studio 3.0.1.0. The problem was resolved by using CrossCore Embedded Studio 2.12.1, which successfully compiled and loaded the firmware on both Windows and Linux. The user also confirmed that the original CN0359.bin file worked correctly, suggesting the issue was with the firmware generation in the newer CCES version.
AI Generated Content
Category: Software

Hello all, i have some problems starting up with the conductivity measurement module

            We have  EVAL-CN0359-EB1Z Rev. A  evaluation board. We intend to use it in outr production. I have installed  CrossCore Embedded Studio 3.0.1.0. on windows 10

            I followed the steps  https://wiki.analog.com/resources/eval/user-guides/circuits-from-the-lab/cn0359            i have done:

Software Development Environment

Rev A Source Code

Click to hide ⇱ 

The source code for the CN0359 software can be downloaded from: EVAL-ADICUP360/tree/master/projects/ADuCM360_demo_cn0359_reva.

ADuCM360_demo_cn0359_reva is a CrossCore project. Import the project in ADI CrossCore Embedded Studio to build and debug the code.

 I have compiled  ADuCM360_demo_cn0359_reva.bin. Following the instructions  https://wiki.analog.com/resources/eval/user-guides/circuits-from-the-lab/cn0359         we have done

Downloading the Firmware to the CN0359

To download the firmware to the CN0359 evaluation board:

  1. Download and install the latest J-Link Software and Documentation Pack.

2a. For Rev A evaluation boards:

We load in the kit the compilled from us file  ADuCM360_demo_cn0359_reva.bin. The kit is not working - no messages on the display, no nothing, does not react on the rs interface. When we follow the same steps but load cn0359-DesignSupport\EVAL-CN0359-EB1Z Rev. A\CN0359 RevA Source Code\Release\CN0359.bin (downloaded from the previous EVAL-CN0359 :

https://wiki.analog.com/resources/eval/user-guides/circuits-from-the-lab/cn0359?rev=1627542821#how_to_download_binary_firmware_to_the_cn0359      ),we see that the kit works properly. We think we are following the same instructions in loading so where might be the problem? How to properly generate the  .bin file.

            Any kind of help would be much appreciated

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.