Post Go back to editing

EV_FLOWMETER-ARDZ BOARD (MAX35101) CONFIGURATION SUPPORT

Thread Summary

The user is facing issues configuring the EV FLOWMETER ARDZ board with the MAX35101 for flow measurement using Arduino Uno via SPI. The board is not responding and not providing proper data. The final answer suggests checking the register configurations in the folder C:\Analog Devices\AD-MAX32WISE-SLZ-Rel1.0.0\Software\ad_max32wise_src\no-os\project\flow_meter for additional reference. The user also mentions issues with the ultrasonic pulse detection and requests guidance on setting the comparator offset voltage and selecting an appropriate ultrasonic transducer for water.
AI Generated Content
Category: Hardware
Product Number: MAX35101

I am facing issue regarding the configuration of EV FLOWMETER ARDZ board with MAX35101 used for flow measurement. I try to program this board using Arduino uno via SPI communicaton, but the board is not responding and not giving the proper data. So t will be very helpful if anyone helps me to solve this.

Parents Reply
  • I Used a 1.2k and 2.4k resistor in series to build a voltage divider which converst 5v to 3.3v. I used these for MOSI,SCK,and CS line. Not used for MISO line. 
    But the main problem I am facing is on detecting the signal which is produced by the transducer. Actually the signal is received at the receiver transducer when checked using an oscilloscope ,but the issue is this is not detected by the MAX35101 as an ultrasonic pulse. Could you please provide a configuration that properly works on this IC.Or could you help me to how to set comparator offset voltage.

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.