Post Go back to editing

EV_FLOWMETER-ARDZ BOARD (MAX35101) CONFIGURATION SUPPORT

Thread Summary

The user is facing issues configuring the EV FLOWMETER ARDZ board with the MAX35101 for flow measurement using Arduino Uno via SPI. The board is not responding and not providing proper data. The final answer suggests checking the register configurations in the folder C:\Analog Devices\AD-MAX32WISE-SLZ-Rel1.0.0\Software\ad_max32wise_src\no-os\project\flow_meter for additional reference. The user also mentions issues with the ultrasonic pulse detection and requests guidance on setting the comparator offset voltage and selecting an appropriate ultrasonic transducer for water.
AI Generated Content
Category: Hardware
Product Number: MAX35101

I am facing issue regarding the configuration of EV FLOWMETER ARDZ board with MAX35101 used for flow measurement. I try to program this board using Arduino uno via SPI communicaton, but the board is not responding and not giving the proper data. So t will be very helpful if anyone helps me to solve this.

Parents Reply Children
No Data